Question, i.MX6UltraLight DDR3L configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6UltraLight DDR3L configuration

387 Views
SLICE
Contributor IV

Dear team,

I would like to ask about DDR memory connection for i.MX6UltraLight.

My customer wants to create 2GByte memory space by using 2 chips of DDR3Ls.

They think the following 2 ways are allowable for i.MX6UL.

[8Gb x8bit data width x2, 1 rank]

[8Gb x16bit data width x2, 2 rank]

Is it true?

If you have any concerns on that, please let me know.

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Reply

280 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

seems second option implies twin die memory like

MT41K512M16 – 32 Meg x 16 x 8 Banks x 2 Ranks,

both options memory connections are allowable.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos