Question, i.MX6ULL NVCC_xxx voltage

cancel
Showing results for 
Search instead for 
Did you mean: 

Question, i.MX6ULL NVCC_xxx voltage

297 Views
Aemj
Contributor IV

Dear team,

I would like to ask a quick question about voltage of i.MX6ULL NVCC_xxx.

Can I understand that IO voltage of Quad SPI NOR Flash connected to i.MX6ULL will be 3.3V in the case of feeding 3.3V into NVCC_xxx of i.MX6ULL?

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Reply

198 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Miyamoto

>Can I understand that IO voltage of Quad SPI NOR Flash connected to i.MX6ULL

>will be 3.3V in the case of feeding 3.3V into NVCC_xxx of i.MX6ULL?

yes this is right understanding.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos