Question, i.MX6SoloX U-Boot with eMMC fastboot enabled

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question, i.MX6SoloX U-Boot with eMMC fastboot enabled

1,523 次查看
SLICE
Contributor IV

Dear team,

Let me ask about how to build U-Boot with enabling eMMC Fast boot mode.

My customer is facing to build u-boot.

They want to be sure that the u-boot has a feature for load kernel image with eMMC fastboot.

They found a definition of “CONFIG_FSL_FASTBOOT” in your u-boot source code including your following BSP code. (in mx6sxsabresd.c)

git://git.freescale.com/imx/fsl-arm-yocto-bsp.git -b imx-3.14.52-1.1.0_ga

And they think that CONFIG_FSL_FASTBOOT should be defined for u-boot to have a feature to load kernel image with eMMC fastboot.

Is it true?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 回复

1,216 次查看
art
NXP Employee
NXP Employee

Actually, this feature is still not confirmed as being reliably supported in the current versions of software, so, it is not recommended to use it at all.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复