Question, i.MX6Solo parallel camera input port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6Solo parallel camera input port

1,057 Views
Aemj
Contributor IV


Dear team,

My customer wants to use Maxim/MAX9272, Deserializer, for camera input of i.MX6Solo.

As for the parallel output from MAX9272, a spread spectrum(1%) is added.

Can i.MX6SL receive the parallel data from MX9271 correctly?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
3 Replies

907 Views
art
NXP Employee
NXP Employee

Yes, it is possible to use the MAX9272 on the parallel CSI input port of i.MX6SL with 1% spread spectrum on pixel clock/output. Also, please note that the CSI port of i.MX6SL is maximum 16-bit wide, so, the corresponding data format should be selected on the link/deserializer side.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

907 Views
Aemj
Contributor IV

Hi Artur,

Thanks for your answer.

Can i understand that there is no special setting for i.MX6 to receive 1% SS signal?

Thanks,

Miyamoto

0 Kudos
Reply

907 Views
art
NXP Employee
NXP Employee

No, no special settings are required for i.MX6 to get the 1% spread spectrum CSI input.

Best Regards,

Artur

0 Kudos
Reply