Question, i.MX6SX/errata ERR009572

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6SX/errata ERR009572

986 Views
Aemj
Contributor IV

Dear team,

I would like to ask about ERR009572 of i.MX6SX.

My customer found ERR009572 in your latest (Rev.1) errata document of i.MX6SX.

They are working on the similar issue on their proto-board.

The chip parts# which they are using is MCIMX6X3EVK10AB and the date-code is 1525.

As for the description on the errata document, they understand it as below.

If the date-code is bigger than 1524, PCIE_DISABLE fuse is not burned during your manufacturing process. And the issue does not occur.

Is it true?

Thanks,

Miyamoto

Labels (1)
0 Kudos
4 Replies

760 Views
subzero
Contributor I

hello Igor,

i have a similar issue as above, assuming that the  MCIMX6X3EVK10AB with the date-code 1525 is fixed similar as the 1533, why is it when i access the RDC register it failed on 1525 but not 1533?

I had build a simple helloworld using the MQX 4.1  for both the solox sabre sd and my custom board, both has only the uart1 and the qspi enable in uboot, but the custom board with 1525 failed at RDC access.

Custom Board(1525):

=> md 0x20FC204
020fc204: <<--Uboot hangs

SoloX sabre SD (1533):

Word 0x00000000: 00000000
=> md 0x20FC204
020fc204: 00000000 00000000 00000000 00000000 ................
020fc214: 00000000 00000000 00000000 00000000 ................
020fc224: 00000000 00000000 00000000 00000000 ................
020fc234: 00000000 00000000 00000000 00000000 ................
020fc244: 00000000 00000000 00000000 00000000 ................
020fc254: 00000000 00000000 00000000 00000000 ................
020fc264: 00000000 00000000 00000000 00000000 ................
020fc274: 00000000 00000000 00000000 00000000 ................
020fc284: 00000000 00000000 00000000 00000000 ................
020fc294: 00000000 00000000 00000000 00000000 ................
020fc2a4: 00000000 00000000 00000000 00000000 ................
020fc2b4: 00000000 00000000 00000000 00000000 ................
020fc2c4: 00000000 00000000 00000000 00000000 ................
020fc2d4: 00000000 00000000 00000000 00000000 ................
020fc2e4: 00000000 00000000 00000000 00000000 ................
020fc2f4: 00000000 00000000 00000000 00000000 ................
=>  <<-- Uboot ok

Hope that you could assist me, Thank you.

Best Regards,

Andy

0 Kudos

760 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

yes this is right understanding

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

760 Views
Aemj
Contributor IV

Hello Igor,

Thanks for your support.

The customer is using MCIMX6X3EVK10AB with the date-code 1525, but the issue occurs on the customer's board.

Could you show me how to read the PCIE_DISABLE fuse value?

They want to check if the fuse are blown or not, but they could not find the location of PCIE_DISABLE on fuse-map in your reference manual.

Thanks,

Miyamoto

0 Kudos

760 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

please create service request.

Best regards
igor

0 Kudos