Question, i.MX6Q SATA_PHY_7 settings

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6Q SATA_PHY_7 settings

Jump to solution
534 Views
Aemj
Contributor IV

Dear team,

I would like to ask about the loss of signal detection level of i.MX6Q/SATA.

In the reference manual of i.MX6Q, the following is written as the description for SATA_PHY_7.

SATA1i

SATA1m

SATA1x

SATA2i

SATA2m

SATA2x

Could you show me what the SATA1i-SATA2x stand for?

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Solution
456 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

this is usage model, one can look at Table 2: General Specifications

http://www.csit-sun.pub.ro/~cpop/Documentatie_SM/Standarde_magistrale/SATA/PHYii%20Spec%20Rev%201_0%...

Best regards

igor
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
457 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

this is usage model, one can look at Table 2: General Specifications

http://www.csit-sun.pub.ro/~cpop/Documentatie_SM/Standarde_magistrale/SATA/PHYii%20Spec%20Rev%201_0%...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos