Hi,
there is only one MAC in i.MX6Q, so you counldn't use MII and RGMII at the same time.
Have a great day,
TIC weidong sun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello weidong.sun
Thanks for your support.
Actually, the customer already has an experience to use below signals for 100-base Ethernet connection. They verified its behavior on their first proto board.
- ENET_MDC
- ENET_MDIO
- ENET_CRS_DV
- ENET_REF_CLK
- ENET_RXD0
- ENET_RXD1
- ENET_TXD0
- ENET_TXD1
- ENET_RX_ER
- ENET_TX_ER
The above situation shows that SGMII interface signals can be left free even while 100Base Ethernet is used.
Then the customer thinks that 100base Ethernet(not GIGA-Ether) and RGMII (for the other purpose) can be used simultaneously.
But I think that MAC should be used if one uses RGMII or MII even for other purpose.
So, if one needs to use Ethernet(100base or GIGA), RGMII and MII interface cannot be used for the other purpose.
Correct?
Best Regards,
Miyamoto
Hello Masamichi,
MAC in i.MX6 can support MII / RGMII / RMII, customer can only select one of them for her application. She can't use any two of them at the same time.
Best regards,
Weidong sun
Hello weidong.sun
Thanks for you help.
I believe using MII nor RGMII for other purpose than Ethernet under the situation that MAC is used for LAN is impossible.
Right?
Thanks,
Miyamoto