Question, i.MX6DQ ripple noise on power rails

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question, i.MX6DQ ripple noise on power rails

跳至解决方案
1,444 次查看
Aemj
Contributor IV

Hi team,

I would like to ask about the ripple noise for i.MX6DQ power rails.

I found the description as below in i.MX6DQ hardware development guide.

“Common requirement for ripple noise should be less than 5% Vp-p of supply voltage average value.

Related power rails affected: all VDD_xxx_IN and VDD_xxx_CAP.”

How about the other NVCC_XXX power rails than VDD_xxx_IN and VDD_xxx_CAP?

Thanks,

Miyamoto

标签 (2)
0 项奖励
回复
1 解答
1,381 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

there are no requirement for ripple noise for NVCC_XXX,

only requirement is that  these voltages should be within ranges

specified by datasheet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,382 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

there are no requirement for ripple noise for NVCC_XXX,

only requirement is that  these voltages should be within ranges

specified by datasheet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,381 次查看
mythilir
Contributor I

Hi,

I am using IMX6Q Sabre-Lite board. In that board there is a power short between 5v and ground section.The power indicating LED is blinking when connected to the supply.How can we fix this?

Kindly suggest the way to resolve the same.

0 项奖励
回复