Question, i.MX6DQ ripple noise on power rails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6DQ ripple noise on power rails

ソリューションへジャンプ
1,513件の閲覧回数
Aemj
Contributor IV

Hi team,

I would like to ask about the ripple noise for i.MX6DQ power rails.

I found the description as below in i.MX6DQ hardware development guide.

“Common requirement for ripple noise should be less than 5% Vp-p of supply voltage average value.

Related power rails affected: all VDD_xxx_IN and VDD_xxx_CAP.”

How about the other NVCC_XXX power rails than VDD_xxx_IN and VDD_xxx_CAP?

Thanks,

Miyamoto

ラベル(2)
0 件の賞賛
返信
1 解決策
1,450件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

there are no requirement for ripple noise for NVCC_XXX,

only requirement is that  these voltages should be within ranges

specified by datasheet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,451件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

there are no requirement for ripple noise for NVCC_XXX,

only requirement is that  these voltages should be within ranges

specified by datasheet.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,450件の閲覧回数
mythilir
Contributor I

Hi,

I am using IMX6Q Sabre-Lite board. In that board there is a power short between 5v and ground section.The power indicating LED is blinking when connected to the supply.How can we fix this?

Kindly suggest the way to resolve the same.

0 件の賞賛
返信