Question, i.MX6DQ DDR_SEL setting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6DQ DDR_SEL setting

Jump to solution
844 Views
Aemj
Contributor IV

Hi All,

I would like to ask about IOMUXC_SW_PAD_CTL_GRP_DDR_TYPE_RGMII register of i.MX6DQ.

Should one set 11b into the DDR_SEL field in the case of using 1.8V/2.5V PHY?

Or, can DDR_SEL be default value(10b) regardless of the IO voltage of PHY?

Please give your answer to the above, and the explanation about this DDR_SEL setting as well.

BR,

Miyamoto

Labels (2)
0 Kudos
Reply
1 Solution
693 Views
Yuri
NXP Employee
NXP Employee

DDR_SEL should be set as 11 for RGMII interface (for signals ranging from 1.3V to 2.5V). 

View solution in original post

0 Kudos
Reply
1 Reply
694 Views
Yuri
NXP Employee
NXP Employee

DDR_SEL should be set as 11 for RGMII interface (for signals ranging from 1.3V to 2.5V). 

0 Kudos
Reply