Question, i.MX53 ERR009348

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX53 ERR009348

Jump to solution
653 Views
Aemj
Contributor IV

Dear team,

I would like to ask about ERR009348(FlexCAN) of i.MX53.

Is this erratum effective for i.MX535?

And can i understand that this erratum can be ignored if FlexCAN module of i.MX535 is not used?

Thanks,

Miyamoto

Labels (1)
0 Kudos
1 Solution
549 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

     In i.mx535, there are no Flex CAN bus IP modules. It means I.MX535 doesn't support CAN BUS. If customer wants to use Flex CAN bus, she should select other i.MX53 series SoC, such as i.mx536/537/534.

 

Best Regards,

Weidong

View solution in original post

0 Kudos
1 Reply
550 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

     In i.mx535, there are no Flex CAN bus IP modules. It means I.MX535 doesn't support CAN BUS. If customer wants to use Flex CAN bus, she should select other i.MX53 series SoC, such as i.mx536/537/534.

 

Best Regards,

Weidong

0 Kudos