Question, i.MX53 ERR009348

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX53 ERR009348

ソリューションへジャンプ
650件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about ERR009348(FlexCAN) of i.MX53.

Is this erratum effective for i.MX535?

And can i understand that this erratum can be ignored if FlexCAN module of i.MX535 is not used?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
1 解決策
546件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

     In i.mx535, there are no Flex CAN bus IP modules. It means I.MX535 doesn't support CAN BUS. If customer wants to use Flex CAN bus, she should select other i.MX53 series SoC, such as i.mx536/537/534.

 

Best Regards,

Weidong

元の投稿で解決策を見る

0 件の賞賛
1 返信
547件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Miyamoto,

     In i.mx535, there are no Flex CAN bus IP modules. It means I.MX535 doesn't support CAN BUS. If customer wants to use Flex CAN bus, she should select other i.MX53 series SoC, such as i.mx536/537/534.

 

Best Regards,

Weidong

0 件の賞賛