Question, i.MX283 thermal characteristic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX283 thermal characteristic

Jump to solution
609 Views
Aemj
Contributor IV

Dear team,

I would like to ask about the thermal characteristic of i.MX283.

My customer is evaluating MCIMX283DVM4B on his board and has a question on the thermal characteristics of i.MX28.

In their test, the temperature of i.MX28 surface reached 64 degrees C when the environmental temperature was 25 degrees C.

At that time, the usage rate of i.MX283 was 50%.

CHSimbolmeasurement pointTemp. Deg.CEstimated DegC in 45 DegC of environmentalMax.Ratings
CH1U1surface of i.MX28363.884.170


The power consumption of DC24V on the board is 140-150mA.

Is that reasonable?

Do you have any ideas to lower the temperature?

Estimated temp number in the 45 degrees C of the environmental temp is 84 degrees C, and the number exceeds the maximum ratings.

The customer has a doubt whether the temp really can reach to 64 even when the usage rate was 50%.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
542 Views
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

this depends on many factors, in particular how i.MX28 is powered.

If it is powered from 5V then I think it can easily reach such temperature:

5V*0.15A=0.75W  RθJA=36C/W , "four layer board (2s2p)" (Table 21 IMX28CEC )

delta T = 0.75W * 36C/W= 27C --> 25 +27 =52C

For minimizing temperature it is recommended to use power from DCDC_BATT.

Best regards

igor

View solution in original post

0 Kudos
Reply
1 Reply
543 Views
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

this depends on many factors, in particular how i.MX28 is powered.

If it is powered from 5V then I think it can easily reach such temperature:

5V*0.15A=0.75W  RθJA=36C/W , "four layer board (2s2p)" (Table 21 IMX28CEC )

delta T = 0.75W * 36C/W= 27C --> 25 +27 =52C

For minimizing temperature it is recommended to use power from DCDC_BATT.

Best regards

igor

0 Kudos
Reply