hi team,
I would like to ask about the handling of the following unused pins.
- TAMPER_A/B
- MECH_C/D
- XP/XN
- YP/YN
My customer thinks those pins should be pulled to high when unused for security.
If so, could you show me what register value should be used for pull-up?
Thanks,
Miyamoto
According to section 2.1 (Special Signal Considerations) of the i.MX25 Datasheet :
TAMPER_A/B and MECH_C/D pins can be left unconnected if the DryIce security
features are not being used.
http://cache.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf
When not used, XP, XN, YP, YN also may be left free.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------