Question, i.MX25 KPP port usage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX25 KPP port usage

Jump to solution
2,326 Views
Aemj
Contributor IV

Hi team,

I would like to ask about KPP port of i.MX25.

My customer plans to use KPP_ROW6(V5 pin) port of i.MX257 as a GPIO output.

The customer believes that the KPP_ROW6 pin can be used to output High or Low at any desired timing.

Is it true?

Please let me know if you have any concern on that.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
2,125 Views
Yuri
NXP Employee
NXP Employee

Hello,

KPP_ROW6 (V5) pin has no GPIO functionality as Fabio mentioned.

Nevertheless, You are right, the KPP in itself allows to control pin state.

KPCR[KRE6] = 0 (Row is not included in the keypad key press detect)

KDDR[KRDD6] = 1 (ROW pin configured as an output)

KPDR[KRD6] = 1/0 (data)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
2,125 Views
fabio_estevam
NXP Employee
NXP Employee

There is no GPIO functionality associated with this particular pin.

Regards,

Fabio Estevam

0 Kudos
Reply
2,125 Views
Aemj
Contributor IV

Hi Fabio,

Thanks for your reply but I need more detailed explanation on that.

I think the port, KPP_ROW6, can be configured as an output port by configuring Keypad Data Direction Register (KDDR).

And I think one can control the output level of KPP_ROW6 by writing 1 or 0 bit into KPDR[6].

Am I wrong?

Thanks,

Miyamoto

0 Kudos
Reply
2,126 Views
Yuri
NXP Employee
NXP Employee

Hello,

KPP_ROW6 (V5) pin has no GPIO functionality as Fabio mentioned.

Nevertheless, You are right, the KPP in itself allows to control pin state.

KPCR[KRE6] = 0 (Row is not included in the keypad key press detect)

KDDR[KRDD6] = 1 (ROW pin configured as an output)

KPDR[KRD6] = 1/0 (data)


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,125 Views
Aemj
Contributor IV

Hi team,

The reference manual of i.MX25 says as below.

"The kKeypad port (KPP) is a 16-bit peripheral that can be used as a keypad matrix interface or as general

purpose input/output (I/O)."

Could you give your detailed reason why you say that KPP_ROW6 (V5) pin has no GPIO functionality?

Thanks,

Miyamoto

0 Kudos
Reply
2,125 Views
Yuri
NXP Employee
NXP Employee

Hello,

> why you say that KPP_ROW6 (V5) pin has no GPIO functionality?

Most of KPP signals can be configured as GPIO via IOMUXC_SW_MUX_CTL_PAD_KPP-...

registers, but the KPP_ROW6 does not have corresponding register.


   Only the following ones are available : 

IOMUXC_SW_MUX_CTL_PAD_KPP_ROW0

IOMUXC_SW_MUX_CTL_PAD_KPP_ROW1

IOMUXC_SW_MUX_CTL_PAD_KPP_ROW2

IOMUXC_SW_MUX_CTL_PAD_KPP_ROW3

IOMUXC_SW_MUX_CTL_PAD_KPP_COL0

IOMUXC_SW_MUX_CTL_PAD_KPP_COL1

IOMUXC_SW_MUX_CTL_PAD_KPP_COL2

IOMUXC_SW_MUX_CTL_PAD_KPP_COL3

Regards,

Yuri.

0 Kudos
Reply
2,125 Views
fabio_estevam
NXP Employee
NXP Employee

Now I see the response from Yuri and understood that it is possible to program the KPP interface to use the pin as an output.

Sorry for the confusion.

Regards,

Fabio Estevam

0 Kudos
Reply