Dear team,
I would like to ask about analog input pins of i.MX25.
(1)
Can I understand that the maximum input range of INAUXx pins of i.MX25 is NVCC_ADC+0.3V?
(2)
My customer plans to rise NVCC_ADC at 1mS after the rising of NVDD_GPIO on their i.MX25 board.
The both of the voltage level are 3.3V.
Is it possible to input 3.3V into INAUXx pins during the 1mS, before the rising of NVCC_ADC and after the rising of NVDD_GPIO?
I think that the 3.3V into INAUXx pins has to be input after the rising of NVCC_ADC.
Thanks,
Miyamoto
Solved! Go to Solution.
Hi Miyamoto
1. yes
2. >I think that the 3.3V into INAUXx pins has to be input after the rising of NVCC_ADC
correct, external voltages should not be applied to processor (module) when it did
not complete power-up sequence.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Miyamoto
1. yes
2. >I think that the 3.3V into INAUXx pins has to be input after the rising of NVCC_ADC
correct, external voltages should not be applied to processor (module) when it did
not complete power-up sequence.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------