Question, i.MX25 ADC characteristic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX25 ADC characteristic

864 Views
Aemj
Contributor IV

Dear team,

My customer will develop a software using i.MX25 ADC, actually they are about to use XP, XN, YP and YN pins.

They are reading your AN3948 and AN2438 application Notes to understand the ADC behavior. But they want to obtain additional information about the characteristic of ADC conversion.

Do you have any documents which describe about the actual characteristics on the relationship between input voltage and the translated digital value?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Reply

767 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

please check AN3948 i.MX25 Integrated Analog-to-Digital Converter

http://cache.freescale.com/files/dsp/doc/app_note/AN3948.pdf 

and Datasheet, Reference Manual ADC Chapters, I am afraid other

documentation is not available

i.MX25 Reference Manual

http://www.freescale.com/files/dsp/doc/ref_manual/IMX25RM.pdf

i.MX25 Datasheet

http://www.freescale.com/files/dsp/doc/data_sheet/IMX25CEC.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply