Question for the Number of images that can be simultaneously decoded in i.MX8MQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question for the Number of images that can be simultaneously decoded in i.MX8MQ

2,268件の閲覧回数
eric_kang
Contributor II

Dear All,

I want to know the Number of images that can be simultaneously decoded in i.MX8MQ.
Could you tell me the number?

Our test environment is like as below.
For Video Display, we have to make the One-Display image with 4-channels or 8-channels.
So we need to check the Number of images that can be simultaneously decoded in i.MX8MQ.

- MPU : i.MX8MQ
- Video Input
  . Interface : Gigabit Ethernet
  . Encoding : H.264 or H.265
  . Video Resolution : No Fixed
- Video Save
  . Interface : PCIe for HDD/SDD
- Video Output
  . Image : One Display with 4-channel or 8-channel
  . Interface : HDMI / 4K(4096x2160)@60Hz
  . Video Resolution : 4K(4096x2160)@60Hz

- Block Diagram

  . IDIS_NVR.DVR.i.MX_01-4_Block.Diagram_DVR.png

Best Regards,
Eric.

ラベル(2)
タグ(2)
0 件の賞賛
返信
5 返答(返信)

2,115件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Eric,

 I will confirm it for you, and give you reply as soon as possible.

Have a nice day

Rita

0 件の賞賛
返信

2,115件の閲覧回数
eric_kang
Contributor II

Hi Rita Wang,

Please let me know if you have any update.

Best Regards,

Eric.

0 件の賞賛
返信

2,115件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Eric,

So sorry for late reply. I have confirmed, and here could you tell me more, if you want to ask max number can display on screen or the multiple videos overlay?

About the VPU decode, it depend on the video you want to play back.

Have a nice day

Rita

0 件の賞賛
返信

2,115件の閲覧回数
eric_kang
Contributor II

Dear Rita,
Thanks for your Interest.

We have to display the 4-channels or 8-channels video in the same ONE display.
So I think we need to decode the multiple videos in the same time.
And the output display resolution via HDMI is 4K(4096x2160)@60Hz.

In this case, I want to know the below items.
- What is the each resolution for the 4-channels display?
- What is the each resolution for the 8-channels display?

For example,
Output Display Resolution = 4K(4096x2160)@60Hz
4-channels Reslution for this situation = (2048x1080)@60Hz = 4K(4096x2160) / 2
8-channels Reslution for this situation = (1024x 540)@60Hz = 4K(4096x2160) / 4

Best Regards,
Eric.

0 件の賞賛
返信

2,115件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Eric,

The MIPI DSI display the i.M8MQ bandwidth supports up to 1.5Gbps per laneX4lane=6Gbps

Have a nice day

Rita

0 件の賞賛
返信