Question, an accuracy of i.MX28 Internal DC/DC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, an accuracy of i.MX28 Internal DC/DC

898 Views
SLICE
Contributor IV

Dear team,

According to i.MX28 datasheet, the accuracy of its internal DC/DC is +-3% when there is no load.

Do you have any accuracy data of DC/DC of when there are loads?

My customer is using i.MX28 and they found the accuracy (when there are loads) got lower than the mention of datasheet.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Reply

784 Views
art
NXP Employee
NXP Employee

The typical accuracy of the i.MX28 DC/DC converter under normal load conditions (as specified in the datasheet) and specified external components, i.e. 15uH inductor and at least 33uF of bulk capacitance (typical configuration is 22uF + 10uF + 1uF + 0.1uF + 0.01uF low ESR capacitors in parallel), is +/- 5% .


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply