Question about operation when user want to transfer more than 4KB data from EEPROM at boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about operation when user want to transfer more than 4KB data from EEPROM at boot

跳至解决方案
1,051 次查看
ko-hey
Senior Contributor II

Hi everyone,

 

I have a question about the operation when I want to transfer more than 4KB of data from EEPROM at boot time.

There is the following description in reference manual after copying 4KB of data from EEPROM to internal RAM by the boot ROM code.

 

6.1.5.5.1 Serial(SPI) NOR eFUSE configuration

After a successful DCD extraction, the ROM code

extracts the destination pointer and length of image from the Boot Data Structure to be

copied to the RAM device from where the code execution occurs.

 

6.1.5.5.2 ECSPI boot

If the DCD verification is successful, the ROM code copies the initial 4 KB of data, as

well as the rest of the image extracted from the application image, directly to the

application destination.

 

Question)

The information contained in the initially transferred 4KB data is analyzed, and the portion exceeding 4KB is automatically copied.

Am I correct ?

 

Ko-hey

标签 (1)
0 项奖励
回复
1 解答
1,031 次查看
Yuri
NXP Employee
NXP Employee

ko-hey 

Hello,

  Correct - the information contained in the initially transferred 4KB data is analyzed, and the portion exceeding

4KB is automatically copied.

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,032 次查看
Yuri
NXP Employee
NXP Employee

ko-hey 

Hello,

  Correct - the information contained in the initially transferred 4KB data is analyzed, and the portion exceeding

4KB is automatically copied.

Regards,

Yuri.

0 项奖励
回复