Question about i.MX53 DDR3 Script Aid

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question about i.MX53 DDR3 Script Aid

1,540 次查看
ko-hey
Senior Contributor II

Hi all

I want to confirm about i.MX53 DDR3 Script Aid.

I downloaded it from below thread.

https://community.freescale.com/docs/DOC-102457

In my understanding, if user set some information in "Register Configuration" tab, the register values are changed in "RealView.inc" tab.

But some register values are never changed (e,g ESDREF).

Does it proper operation ?

If you know something about it, please tell me.

ko-hey

标签 (1)
标记 (2)
0 项奖励
回复
4 回复数

1,173 次查看
Yuri
NXP Employee
NXP Employee

Yes, the i.MX53 DDR3 Script Aid is very simplified, and it does not

support fine tuning of DDR parameters.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,173 次查看
ko-hey
Senior Contributor II

Hi Yuri

So user have to change themselves ?

Ko-hey

0 项奖励
回复

1,173 次查看
Yuri
NXP Employee
NXP Employee

You can request more detailed xls via SR.

Regards,

Yuri.

0 项奖励
回复

1,173 次查看
ko-hey
Senior Contributor II

OK, I'll ask to SR.

ko-hey

0 项奖励
回复