Question about armel/armhf toolchain on Yocto for imx6

cancel
Showing results for 
Search instead for 
Did you mean: 

Question about armel/armhf toolchain on Yocto for imx6

858 Views
brianwu
Contributor III

Hi community,

The default setting use the armhf toolchain for imx6 on Yocto (daisy/dora branch), so the FAE suggest us to use the armhf toolchain.

I have a customer using the armel toolchain and the FAE worry the armel toolchain will cause some problems on GPU part,

My question:

1. Do the community also suggest to use the armhf toolchain?

2. If yes, why?

BR

Brian

Labels (2)
0 Kudos
1 Reply

160 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi brianwu

1. yes, suggested to use armhf

2. main reason is improving performance, also one can look below

armhf libraries for imx6

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos