Question about VPU EncOpenParam

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about VPU EncOpenParam

跳至解决方案
1,701 次查看
ko-hey
Senior Contributor II

Hi all,

 

 

Let me ask about a EncOpenParam for VPU operation.

 

Q1.

If EncOpenParam's bitRate is set to something other than "0", will it exceed the specified bitRate?

* Will it be controlled at a fixed bit rate?

 

Q2.

If EncOpenParam's bitRate is specified with something other than "0", will it compensate to the specified bit rate with padding when the bit rate is less than the bit rate specified at encoding?

 

Q3.

Does userOpMax and userQpMin set the fluctuation range of the Q value in units of macroblocks?

 

 

Ko-hey

0 项奖励
回复
1 解答
1,542 次查看
joanxie
NXP TechSupport
NXP TechSupport

for bitrate, which depends on what mode you use, if you use CBR, yes, you can set the fixed bitrate

what do you mean userOpMax  and Q value? do you mean QP value?

if yes, refer to the VPU  API reference manual, pMBQpInfo is not used in imx6

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,542 次查看
ko-hey
Senior Contributor II

Hi all

Could someone follow and answer this thread ?

Ko-hey

0 项奖励
回复
1,543 次查看
joanxie
NXP TechSupport
NXP TechSupport

for bitrate, which depends on what mode you use, if you use CBR, yes, you can set the fixed bitrate

what do you mean userOpMax  and Q value? do you mean QP value?

if yes, refer to the VPU  API reference manual, pMBQpInfo is not used in imx6

0 项奖励
回复