Question about PTM, ETB settings on IMX 6 solox?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about PTM, ETB settings on IMX 6 solox?

600 Views
pung2516
Contributor I

Hi guys, again.

Im trying to use PTM, ETB from my board which is I.MX 6 solox.

I wanna check the packet from ETB.

So Could you guys tell me something specific things(?) or setups that i should do to use PTM for the IMX6solox board?

Tags (1)
0 Kudos
2 Replies

521 Views
igorpadykov
NXP Employee
NXP Employee

Hi Jiwon

one can look on

ARM DS-5 Quick Start (i.MX6) - BlueWiki 

Is it possible to use the CoreSight/PTM on any of the i.MX6 evaluation boards? 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

521 Views
pung2516
Contributor I

Thx for your replying.

I still cannot figure it out.

Im trying to check my ptm trace from the internal ETB without external adaptor such as JTAG.

So could you tell me more about utilizing ETB which is already inside of the IMX6sx board?

0 Kudos