Hello,
i have a question about BOOT_CFG[6:4] Pins from ref-manuel imx8m-mini.
How can i choose a different bus-width for SD-Card (1/4-Bit ) and eMMC (1/4/8-Bit)?
Thanks
Solved! Go to Solution.
Hello Tino,
Yes indeed this table is related to the fuese map, but the definition of the bits used for BOOT_CFG[4:6] are the same even if you are using the GPIO:
For SD/eSD it only use BOOT_CFG[4] for bus width, bits 5 and 6 are reserved
0 - 1 bit
1 - 4 bit
As for MMC/eMMC it uses the 3 bits
000 - 1 bit
001 - 4 bit
010 - 8 bit
011 - reserved
100 - reserved
101 - 4 bit DDR (MMC 4.4)
110 - 8 bit DDR (MMC 4.4)
111 - reserved
Just like in the table above.
Hope this helps,
Best regards,
Aldo.
Hello,
From the reference manual of the i.MX 8MM page 815 and 816
Hope this helps,
Best regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Aldo,
the table 6-42/6-43 is for using fuses.
I wanna use only GPIO boot overrides (BOOT_CFG[4:6]) to change bus width for SD-Card or eMMC.
At this point the table 6-19 is a bit unclear for me.
Best regards,
Tino
Hello Tino,
Yes indeed this table is related to the fuese map, but the definition of the bits used for BOOT_CFG[4:6] are the same even if you are using the GPIO:
For SD/eSD it only use BOOT_CFG[4] for bus width, bits 5 and 6 are reserved
0 - 1 bit
1 - 4 bit
As for MMC/eMMC it uses the 3 bits
000 - 1 bit
001 - 4 bit
010 - 8 bit
011 - reserved
100 - reserved
101 - 4 bit DDR (MMC 4.4)
110 - 8 bit DDR (MMC 4.4)
111 - reserved
Just like in the table above.
Hope this helps,
Best regards,
Aldo.