Question about DDR memory bandwidth of i.MX8MNano

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about DDR memory bandwidth of i.MX8MNano

跳至解决方案
1,536 次查看
ko-hey
Senior Contributor II

Hi everyone,

 

I would like to know the DDR memory bandwidth of i.MX8MNano.

 

Q1.

Generally, users should set the bus priority to achieve high efficiency memory bandwidth.

Can i.MX8MNano set the DDR bus priority by user ? Or Is it fixed ?

 

Q2.

Do you have any data for measured value of DDR bus bandwidth ?

 

Q3.

If Q2 is no, how much should I estimate the measured value ?

I guess it's about 30-40% of theoretical value. Do you agree with it ?

 

 

Ko-hey

标签 (1)
0 项奖励
回复
1 解答
1,468 次查看
art
NXP Employee
NXP Employee

1. The DDR bus priority of the i.MX8MNano processor is fixed to the highest one.

2. No, we don't have any measured numbers of the i.MX8MNano DDR bus bandwidth.

3. Typically, the real DDR bus bandwidth is about the half of the theoretical one.

Best Regards,

Artur

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,469 次查看
art
NXP Employee
NXP Employee

1. The DDR bus priority of the i.MX8MNano processor is fixed to the highest one.

2. No, we don't have any measured numbers of the i.MX8MNano DDR bus bandwidth.

3. Typically, the real DDR bus bandwidth is about the half of the theoretical one.

Best Regards,

Artur

0 项奖励
回复