Question about DDR memory bandwidth of i.MX8MNano

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about DDR memory bandwidth of i.MX8MNano

Jump to solution
1,533 Views
ko-hey
Senior Contributor II

Hi everyone,

 

I would like to know the DDR memory bandwidth of i.MX8MNano.

 

Q1.

Generally, users should set the bus priority to achieve high efficiency memory bandwidth.

Can i.MX8MNano set the DDR bus priority by user ? Or Is it fixed ?

 

Q2.

Do you have any data for measured value of DDR bus bandwidth ?

 

Q3.

If Q2 is no, how much should I estimate the measured value ?

I guess it's about 30-40% of theoretical value. Do you agree with it ?

 

 

Ko-hey

Labels (1)
0 Kudos
Reply
1 Solution
1,465 Views
art
NXP Employee
NXP Employee

1. The DDR bus priority of the i.MX8MNano processor is fixed to the highest one.

2. No, we don't have any measured numbers of the i.MX8MNano DDR bus bandwidth.

3. Typically, the real DDR bus bandwidth is about the half of the theoretical one.

Best Regards,

Artur

View solution in original post

0 Kudos
Reply
1 Reply
1,466 Views
art
NXP Employee
NXP Employee

1. The DDR bus priority of the i.MX8MNano processor is fixed to the highest one.

2. No, we don't have any measured numbers of the i.MX8MNano DDR bus bandwidth.

3. Typically, the real DDR bus bandwidth is about the half of the theoretical one.

Best Regards,

Artur

0 Kudos
Reply