Question, VDD_SOC and VDD_PU of i.MX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, VDD_SOC and VDD_PU of i.MX6DL

1,209 Views
SLICE
Contributor IV

Dear team,

My customer found the following description on your i.MX6Solo/DualLite/Datasheet(IMX6SDLCEC,Rev.9).

“VDD_SOC LDO output set point is equal to the VDD_PU LDO output set point.”

The VDD_PU is the power for graphics feature and they do not use it, then they use the VDD_PU_CAP outputs voltages is about 0.15V and VDD_SOC and VDD_PU is differ.

Is it possible to use VDD_PU as like this even Graphic feature is not used?

Best Regards,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Reply

1,165 Views
Yuri
NXP Employee
NXP Employee

 

Hello,

 

  According to the Datasheet VDD_SOC LDO output set point must be set equal to

the VDD_PU LDO output set point (in LDO enabled mode) without any relation whether

GPU is used or not. 

Have a great day,

Yuri

 

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply