I expect the MIPI CSI-2 interface of the i.MX6 is considered in the thread.
Strictly speaking the mentioned configuration (common clock, two pairs of
data lines from one camera and other two pairs – from the second) is not supported
by the i.MX6 CSI-2 Host Controller, since all the data lines relates to single
camera. Nevertheless Your connection scheme may be implemented, assuming
that only one camera is enabled at time, and the first camera is configured for
two-bits data bus, and the second - for the 4-bits. For the second camera, the
low two bits should be rejected later in software. It may provide some performance
degradation.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------