Qtwebkit and gstreamer on imx6 (yocto Sumo, QT 5.9, framebuffer)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qtwebkit and gstreamer on imx6 (yocto Sumo, QT 5.9, framebuffer)

2,878 Views
gustavevertsson
Contributor I

I am trying to play video in qtwebkit using gstreamer 1.0. I can see that gstreamer get called, plugins is loaded, src and sink is setup etc but then it just stops and no video is showed in the browser. I use the qt5 example browser to test it. I build Sumo yocto without wayland and x11. Is there anything specific that needs to be done to enable this combination? Video plays as it should with gst-play-1.0.

IMAGE_INSTALL_append += "\
    packagegroup-imx-tools-audio \
    imx-codec \
    pulseaudio \
    qtbase-plugins \
    qtbase-tools \
    qtdeclarative \
    qtdeclarative-plugins \
    qtdeclarative-tools \
    qtdeclarative-qmlplugins \
    qtmultimedia \
    qtmultimedia-plugins \
    qtmultimedia-qmlplugins \
    qtsvg \
    qtsvg-plugins \
    qtsensors \
    qtimageformats-plugins \
    qtsystems \
    qtsystems-tools \
    qtsystems-qmlplugins \
    qtscript \
    qt3d \
    qt3d-qmlplugins \
    qt3d-tools \
    qtwebkit \
    qtwebkit-examples-examples \
    qtwebkit-qmlplugins \
    qtgraphicaleffects-qmlplugins \
    qtconnectivity-qmlplugins \
    qtlocation-plugins \
    qtlocation-qmlplugins \
    gstreamer1.0-plugins-imx \
    gstreamer1.0-plugins-imx-meta \
    gstreamer1.0-plugins-bad \
    gstreamer1.0-plugins-base \
    gstreamer1.0-plugins-good \
    packagegroup-fsl-gstreamer1.0 \
    packagegroup-fsl-tools-testapps \
    imx-vpu \
    imx-test \
    firmware-imx-vpu-imx6d \
    "







DISTRO_FEATURES_remove = "X11 wayland"




DISTRO_FEATURES_append = "directfb"
PACKAGECONFIG_append_pn-qtmultimedia = " examples gstreamer"
PACKAGECONFIG_append_pn-qtdeclarative = " qtxmlpatterns"
PACKAGECONFIG_append_pn-qtbase =  "  linuxfb accessibility "
PACKAGECONFIG_remove_pn-gstreamer1.0-plugins-good = " gdk-pixbuf"‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍

The logs ends with these lines. I'm not sure what the timed out at the end means or how to figure out what element/plugin is causing it.

0:00:10.851254563  3447  0x1711600 INFO                 basesrc gstbasesrc.c:1331:gst_base_src_do_seek:<appsrc0> seeking: bytes segment start=0, offset=0, stop=-1, rate=1.000000, applied_rate=1.000000, flags=0x00, time=0, base=0, position 0, duration -1
0:00:10.851607863  3447  0x1711600 INFO                    task gsttask.c:457:gst_task_set_lock: setting stream lock 0x19e0084 on task 0x19f8828
0:00:10.851728851  3447  0x1711600 INFO                GST_PADS gstpad.c:6068:gst_pad_start_task:<appsrc0:src> created task 0x19f8828
0:00:10.852858077  3447  0x1711600 INFO              GST_STATES gstelement.c:2467:gst_element_continue_state:<appsrc0> completed state change to PAUSED
0:00:10.853009062  3447  0x1711600 INFO              GST_STATES gstelement.c:2372:_priv_gst_element_state_changed:<appsrc0> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:10.853207043  3447  0x1711600 INFO              GST_STATES gstbin.c:2945:gst_bin_change_state_func:<source> child 'appsrc0' changed state to 3(PAUSED) successfully
0:00:10.853313033  3447  0x19ace90 INFO        GST_ELEMENT_PADS gstelement.c:915:gst_element_get_static_pad: no such pad 'sink' in element "appsrc0"
0:00:10.853469018  3447  0x1711600 INFO              GST_STATES gstelement.c:2467:gst_element_continue_state:<source> completed state change to PAUSED
0:00:11.185429405  3447  0x19ace90 FIXME                default gstutils.c:3902:gst_pad_create_stream_id_internal:<appsrc0:src> Creating random stream-id, consider implementing a deterministic way of creating a stream-id
0:00:11.185413074  3447  0x1711600 INFO              GST_STATES gstelement.c:2372:_priv_gst_element_state_changed:<source> notifying about state-changed READY to PAUSED (VOID_PENDING pending)
0:00:11.185880696  3447  0x1711600 INFO              GST_STATES gstbin.c:2080:gst_bin_get_state_func:<play> getting state
0:00:11.185991352  3447  0x1711600 INFO              GST_STATES gstelement.c:2185:gst_element_get_state_func:<play> waiting for element to commit state
0:00:11.186134005  3447  0x1711600 INFO              GST_STATES gstelement.c:2199:gst_element_get_state_func:<play> timed out
0:00:11.186456308  3447  0x19ace90 INFO                GST_PADS gstpad.c:4167:gst_pad_peer_query:<typefind:src> pad has no peer

0 Kudos
Reply
3 Replies

1,966 Views
gustavevertsson
Contributor I

We are using the Sumo Yocto build from Congatec as we are using modules from them.

Qseven Computer-On-Modules - congatec AG 

I expected that to include support for graphics acceleration. Was I wrong?

And secondly, running gstreamer stand alone seems to work with graphics acceleration, it it first with combination with qtwebkit that I don't get any output. Do NXP need to add anything to QT for it to work with imx6?

0 Kudos
Reply

1,966 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gustav

Congatec software is supported by Congatec tech support.

Technical Support - congatec AG 

NXP supports only own BSPs described on

i.MX Software|NXP 

NXP software repository

Code Aurora git repositories 

Best regards
igor

0 Kudos
Reply

1,966 Views
igorpadykov
NXP Employee
NXP Employee

Hi Gustav

for sumo nxp have only Linux L4.14.62_1.0.0_Beta:

Linux L4.14.62_1.0.0_Beta Documentation

https://www.nxp.com/webapp/Download?colCode=L4.14.62_1.0.0_Beta_LINUX_DOCS&appType=license&location=... 

linux-imx - i.MX Linux kernel 

one can try with latest GA official release Linux 4.9.88 (rocko)

Linux 4.9.88_2.0.0 BSP & Multimedia Codecs Documentation

https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS&Parent_nodeId=13376994810717061... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply