[Qt5 - iMX6] How to add the support of look and feel of Qt in eglfs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[Qt5 - iMX6] How to add the support of look and feel of Qt in eglfs

562件の閲覧回数
vincentbodin
Contributor II

Hi,

Sorry but maybe this question is probably not in the right place...

I've recently try the QT5Cinematic demo on my iMX6 board through eglfs and it works like a charm.

Now, I'm currently desiging a Qt application with Qwidget support. Unfortunately, when I add a button to the MainWindo.ui, this button doesn't look like it has to be (the look and feel is not very beautiful...). That's the same thing for the Mainwindow.

How to proceed to enable the Qt look and feel in my application ?

Thanks, Vincent

PS : I use the core-image-minimal of Yocto FSL communty BSP

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

402件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vincent

as this is specific Qt question suggest to post it on special Qt forums

like I.MX-6 - Qt Wiki

Best regards

igor

0 件の賞賛
返信