Hi,
i try to run qt on the iMX53 QSB. When i search google or the forum there are links to the old community or imxdev.org. Have somebody a how-to or a discription how to install qt on the QSB?
Edit: I found something, but the link to the attached files is broken. Have somebody the files from this poste? https://community.freescale.com/message/292049#292049
regards,
stefan
解決済! 解決策の投稿を見る。
I'm not sure, but seems you forgot to use:
. ./setup-environment build
before:
bitbake fsl-gui-image
Rgds,
Rogerio
Hi Stefan,
The old page you were looking for is at: https://community.freescale.com/docs/DOC-1481
The information on this page is a bit old and I need to update.
If you want to try, you can also build QT4.8 using Yocto. You only need follow the instructions on page
Freescale/fsl-community-bsp-platform · GitHub
and use the "fsl-image-gui" instead "core-image-minimal". The QT will be built on your image with the demos and examples.
Rgds,
Rogerio
Hi,
thanks for your answers!
I want to try using Yocto, but i get this error. Can you help me with this? i never used yocto before.
lucid@ubuntu:~/fsl-community-bsp$ bitbake fsl-image-gui
Pseudo is not present but is required, building this first before the main build
DEBUG: Removed the following variables from the environment: USERNAME, NO_PROXY, LESSOPEN, LIBGL_ALWAYS_INDIRECT, GNOME_KEYRING_CONTROL, DEFAULTS_PATH, MANDATORY_PATH, WINDOWID, BBFETCH2, GDM_KEYBOARD_LAYOUT, XDG_CONFIG_DIRS, ORBIT_SOCKETDIR, GTK_MODULES, GDMSESSION, LESSCLOSE, OLDPWD, GDM_LANG, SPEECHD_PORT, SHLVL, BUILDDIR, GNOME_DESKTOP_SESSION_ID, LS_COLORS
DEBUG: Found bblayers.conf (/home/lucid/fsl-community-bsp/conf/bblayers.conf)
DEBUG: LOAD /home/lucid/fsl-community-bsp/conf/bblayers.conf
DEBUG: Adding layer /home/lucid/sources/poky/meta
DEBUG: LOAD /home/lucid/sources/poky/meta/conf/layer.conf
ERROR: Unable to parse /home/lucid/sources/poky/meta/conf/layer.conf: [Errno 2] No such file or directory: '/home/lucid/sources/poky/meta/conf/layer.conf'
lucid@ubuntu:~/fsl-community-bsp$
I'm not sure, but seems you forgot to use:
. ./setup-environment build
before:
bitbake fsl-gui-image
Rgds,
Rogerio