Hello,
I am creating a media player application that can play streams from the camera, local files (MP4, MKV), and online streams.
I have got NXP i.MX8M Plus EVK board, and decided to use the Qt framework to develop the application.
I referred to i.MX Yocto Project's User Guide, which guides through the process to create the Linux image using Yocto. I followed all the steps to create a full image (imx-image-full, to include Qt6) for the imx8mp-lpddr4-evk machine, using fsl-imx-wayland distro.
After flashing the image to the board, I ran the video widget sample application provided in Qt6 to play an MP4 file with a resolution of 1920x1080. In an ideal state (video not being played) the CPU consumption remains around 3-5%. However, as soon as the video is played, the CPU consumption shoots to around 50%.
Also, I verified the CPU consumption by playing the same video using a gstreamer pipeline as mentioned in i.MX8 GStreamer User Guide.
gst-launch-1.0 filesrc location=<filename.mp4> ! qtdemux name=d d.video_0 ! queue ! h264parse ! vpudec ! queue ! waylandsink
and
gst-launch-1.0 filesrc location=<filename.mp4> ! qtdemux name=d d.video_0 ! queue ! h264parse ! v4l2h264dec ! imxvideoconvert_g2d ! queue ! waylandsink
The CPU consumption with gstreamer, in both cases, remains around 5% which is 10th of the Qt application.
Here are the questions.
Looking forward to your response to resolve this problem.
Regards,
Aekam Parmar
Hello,
Yes it's normal when working with QT, but the 50% you should be using pure cpu and not gpu, with qtdemux your ensure that you are using qt and gpu.
Regards
I tried running a sample OpenCV application to play a video, to see if it is just Qt or other video processing modules as well that are reporting high CPU usage.
#include "opencv2/opencv.hpp"
#include <iostream>
using namespace std;
using namespace cv;
int main(){
// Create a VideoCapture object and open the input file
// If the input is the web camera, pass 0 instead of the video file name
VideoCapture cap("video.mp4");
// Check if camera opened successfully
if(!cap.isOpened()){
cout << "Error opening video stream or file" << endl;
return -1;
}
while(1){
Mat frame;
// Capture frame-by-frame
cap >> frame;
// If the frame is empty, break immediately
if (frame.empty())
break;
// Display the resulting frame
imshow( "Frame", frame );
// Press ESC on keyboard to exit
char c=(char)waitKey(25);
if(c==27)
break;
}
// When everything done, release the video capture object
cap.release();
// Closes all the frames
destroyAllWindows();
return 0;
}
Also, tried passing a gstreamer pipeline to the VideoCapture.
VideoCapture cap("filesrc video.mp4 ! qtdemux name=d d.video_0 ! queue ! h264parse ! vpudec ! queue ! appsink", CAP_GSTREAMER);
With both options, the application consumes more than 50% CPU.
I am not sure if OpenCV is built to use hardware components.
Please share your opinion on this.
Thank you for the response.