Qt make: g++: Command not found issue with SDK generated for soloX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Qt make: g++: Command not found issue with SDK generated for soloX

跳至解决方案
7,601 次查看
Alankar
Contributor II

i have used following steps to get and build the BSP for soloX sabre board. i am using Krogoth branch to build the bsp and populate sdk

GitHub - Freescale/fsl-community-bsp-platform: BSP platform manifest 

then i added qt support in the build by following 

Building Qt5 using yocto on Wandboard - Wandboard Wiki 

after that i bitbaked toolchain for this using following

$ bitbake meta-toolchain-qt5

after this i generated sdk using following command

$ bitbake <image-name> -c populate_sdk

and then i installed the sdk on my development machine, it is installed under

/opt/poky/2.1.1/

now i installed and setup latest Qt by using following steps

Setup QT Creator with Yocto Build 

After all this setup done, i created a simple console application and trying to build it, and i get an error as

14:10:10: Running steps for project HelloWorld...
14:10:10: Configuration unchanged, skipping qmake step.
14:10:10: Starting: "/usr/bin/make"
g++ -c -pipe -O2 -std=gnu++0x -Wall -W -D_REENTRANT -fPIC -DQT_NO_DEBUG -DQT_CORE_LIB -I../HelloWorld -I. -I/opt/poky/2.1.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/include/qt5 -I/opt/poky/2.1.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/include/qt5/QtCore -I. -I/opt/poky/2.1.1/sysroots/cortexa9hf-neon-poky-linux-gnueabi/usr/lib/qt5/mkspecs/linux-g++ -o main.o ../HelloWorld/main.cpp
make: g++: Command not found
make: *** [main.o] Error 127
14:10:10: The process "/usr/bin/make" exited with code 2.
Error while building/deploying project HelloWorld (kit: mx6solox)
The kit mx6solox has configuration issues which might be the root cause for this problem.
When executing step "Make"
14:10:10: Elapsed time: 00:00.

i have googled a lot but could not find any solution on this.

Can somebody please help on this...

标签 (2)
1 解答
4,903 次查看
Alankar
Contributor II

Hi gusarambula,

i am able to resolve this issue, following are the details

Actually When qmake is run, qtcreator by default puts a “-spec $(QMAKE_XSPEC)” to the argument list. This was causing the compiler now to default to the x86 one instead of the arm one. This was why the compile was failing.

 

The quick fix for this problem is to override the QMAKE_XSPEC variable. This is pretty simple in qtcreator; go to Tools->Options->Build &Run->Kits and add “linux-oe-g++” to the “Qt mkspec” text box.

To add to this, the bug is probably here:

-shortxspec=`echo $XQMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

-shortspec=`echo $QMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

+if [ "$QT_CROSS_COMPILE" = "yes" ] ; then

+    shortxspec=linux-g++

+    shortspec=linux-g++

+else

+    shortxspec=`echo $XQMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

+    shortspec=`echo $QMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

+fi

This is a in a patch file:

/fsl-community-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase /0008-configure-paths-for-target-qmake-properly.patch

and i believe this patch is being applied. i think somebody from Yocto community need to look into this, i will post this to Yocto mailing list also...

Regards...

在原帖中查看解决方案

4 回复数
4,904 次查看
Alankar
Contributor II

Hi gusarambula,

i am able to resolve this issue, following are the details

Actually When qmake is run, qtcreator by default puts a “-spec $(QMAKE_XSPEC)” to the argument list. This was causing the compiler now to default to the x86 one instead of the arm one. This was why the compile was failing.

 

The quick fix for this problem is to override the QMAKE_XSPEC variable. This is pretty simple in qtcreator; go to Tools->Options->Build &Run->Kits and add “linux-oe-g++” to the “Qt mkspec” text box.

To add to this, the bug is probably here:

-shortxspec=`echo $XQMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

-shortspec=`echo $QMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

+if [ "$QT_CROSS_COMPILE" = "yes" ] ; then

+    shortxspec=linux-g++

+    shortspec=linux-g++

+else

+    shortxspec=`echo $XQMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

+    shortspec=`echo $QMAKESPEC | sed "s,^${relpath}/mkspecs/,,"`

+fi

This is a in a patch file:

/fsl-community-bsp/sources/meta-qt5/recipes-qt/qt5/qtbase /0008-configure-paths-for-target-qmake-properly.patch

and i believe this patch is being applied. i think somebody from Yocto community need to look into this, i will post this to Yocto mailing list also...

Regards...

4,903 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Thank you very much for posting your findings, Alankar Dhobale!

0 项奖励
回复
4,902 次查看
raz3l
Contributor III

I have encountered the same problem of Alankar‌. Do you know if this already solved gusarambula‌ or we are supposed to override the QMAKE_XSPEC variable to linux-oe-g++ always now?

0 项奖励
回复
4,903 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Alankar Dhobale,

I have reproduced this error. It’s most likely a Qt Creator configuration issue. I haven’t found a fix but I’ll let you know if I make any progress.

Regards,

0 项奖励
回复