Qt + i.MX53: Linear gradient not working satisfactorily

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qt + i.MX53: Linear gradient not working satisfactorily

1,683 Views
Rooney
Contributor III

Hello!

I'm running a Qt application on the i.MX53 + 10.1" LVDS display. For styling purpose I use a qlineargradient.

QTreeView {
    color: #F0F0F0;
    font-family: MS Shell Dlg 2;
    font-size: 14px;
    font-weight: bold;
    background-color: #B9B9B9;
    background: qlineargradient(x1: 0, y1: 0, x2: 1, y2: 1, stop: 0 #A9A9A9, stop: 1 #C9C9C9);
    border: 1px solid black;
    selection-background-color: transparent;
    border-image: none;
 }

Unfortunately the gradient steps are very distinctiv (see attachment). The second attachment shows the same content on a PC using 32bit graphic.

The LVDS display uses RGB666, so only 18bit is possible.

Is there a way to use qlineargradient that results in same appereance as on the PC? The application would look very simple, if gradients cannot be used.

Thanks für your help!!

Regards,

Rooney

Tags (1)
0 Kudos
Reply
0 Replies