Dear All,
I have been working on a project based on QT-embedded on linux on imx53 sabre platform.
But the problem is qt app does not recognize the touch.... But the touch screen driver is installed
I verified it by doing
export TSLIB_TSDEVICE=/dev/input/ts0
export TSLIB_CALIBFILE=/etc/pointercal
export TSLIB_CONFFILE=/usr/etc/ts.conf
cat /dev/innput/event2 | hexdump
When i do that and touch the screen i get the hex output..... So touch screen is detected by linux.
I have configured the qt-embedded as following.....
./configure -embedded arm -xplatform linux-mxc-g++ -release -prefix /usr/local/Trolltech/Qt-4.6.0/ -no-opengl -glib -qt-gfx-linuxfb -qt-kbd-tty -qt-kbd-linuxinput -qt-mouse-linuxinput -qt-mouse-tslib -little-endian -qt-gfx-linuxfb -host-little-endian -v -opensource -confirm-license -force-pkg-config -no-phonon
so tslib is included.
so how can i make my application get the touch input.. ??
Thanks and regards,
Winston Rodrigues,
Schiller Healthcare
Bangalore
Solved! Go to Solution.
Hi Winston,
It may be the case that the GUI does not know how to interpret the touches. Can you check if the touchscreen driver can be configured/compiled to support SINGLE TOUCH?
Also, Freescale is working on YOCTO, the next BSP builder so I strongly suggest you to try it. It has QT, and the only thing you may need to do is to add a recipe with your custom application. Please take a look at his page to start using it.
Hi Winston,
It may be the case that the GUI does not know how to interpret the touches. Can you check if the touchscreen driver can be configured/compiled to support SINGLE TOUCH?
Also, Freescale is working on YOCTO, the next BSP builder so I strongly suggest you to try it. It has QT, and the only thing you may need to do is to add a recipe with your custom application. Please take a look at his page to start using it.
 
					
				
		
Dear Leonardo...
I dont know exactly how to enable single touch support...
And YOCTO is replacement for LTIB ?
Where can i download the source ?
Thanks,.,.
Winston
 
					
				
		
 Yuri
		
			Yuri
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		 
					
				
		
Dear Yuri Muhin,
I have successfully compiled tslib. and I have set the
environmental variables properly. when I run ./ts_calibrate I can see
"TSLIB calibration Utility" screen on my board. and one crosshair on
top left corner. But when i touch it Nothing happens.
I tried to do a little debugging by using printf statements in
ts_calibrate.c file just to know where exactly is the problem. It gets
struck in the function getxy();
when i see the code of getxy() in tests/testutils.c , it gets
struck at this point :
do {
printf("Inside do-getxy\n");
if (ts_read_raw(ts, &samp[0], 1) < 0) {
printf("Inside if-getxy\n");
perror("ts_read");
close_framebuffer ();
exit(1);
}
} while (samp[0].pressure == 0);
here it never comes out of the do-while loop. so i guess there is a
problem in ts_read_raw() function.
when i run ./ts_print_raw it gives me:
root@freescale /mnt/buha/bin$ ./ts_print_raw
14224.983211: 22304 24288 0
14224.987890: 22304 24288 0
14224.992615: 22304 24288 0
14224.997350: 22304 24288 0
14225.002073: 22304 24288 0
14225.006804: 22304 24288 0
14225.011538: 22304 24288 0
14225.016271: 22304 24288 0
14225.020993: 22336 24272 0
14225.042071: 22432 24272 0
14225.043366: 22432 24272 0
14226.641742: 22544 23968 0
14226.646461: 22544 23968 0
14226.651188: 22544 23968 0
14226.655925: 22544 23968 0
14226.660646: 22544 23968 0
14226.665375: 22544 23968 0
So i guess there is no problem with the touch screen driver.
It uses egalax capacitive touch screen.
Thanks and Regards,
Winston Rodrigues,