Qt-creator setup fro i.mx6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qt-creator setup fro i.mx6

894 Views
nileshkokane
Contributor I
Hi ,


I have a final setup of Qt-creator as follows.I ran the script in the /opt/poky/1.6.1/ and opened the qt-creator from the concole. with this settings as below i'm trying to cross-compile the sample clock code

1. General http://picpaste.com/1-gAmJsS3o.png
2. Kits http://picpaste.com/2-Y3kFvHIG.png
3. Qt version http://picpaste.com/3-lwZngysy.png
4  compiler http://picpaste.com/4-M4y6gJYb.png
5. Debugger http://picpaste.com/5-DQhrxi6t.png
6. CMake   http://picpaste.com/6-l3FhICDq.png
7. Build Settings http://picpaste.com/7-4myooBgL.png

With the settings ,clock code is giving me error[8].

8. http://picpaste.com/8-kGmTWy3P.png

 

14:32:34: Running steps for project clocks...

14:32:34: Could not start process "/opt/poky/1.6.1/sysroots/cortexa9hf-vfp-neon-poky-linux-gnueabi/usr/bin/make" clean

Error while building/deploying project clocks (kit: wandboard)

When executing step 'Make'

14:32:34: Elapsed time: 00:00.


Please if you can assist.

Thanks

Nilesh Kokane

0 Kudos
Reply
0 Replies