Qt 5 is not supported for SoC without hardware graphics???

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Qt 5 is not supported for SoC without hardware graphics???

ソリューションへジャンプ
1,435件の閲覧回数
osmarfrisonjun1
Contributor III

i.MX L3.14.52_1.1.0 GA says the following:

>> Qt 5 is not supported for SoC without hardware graphics. <<

Does it mean that I shouldn't use at the imx6sx?

I have tested it and it seemed to work reasonably.

ラベル(5)
タグ(1)
0 件の賞賛
返信
1 解決策
1,176件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi osmarfrisonjunior2

i.Mx6SX has GPU 2D/3D Vivante GC400T, and yes it support Qt5.

Regards

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,177件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi osmarfrisonjunior2

i.Mx6SX has GPU 2D/3D Vivante GC400T, and yes it support Qt5.

Regards

0 件の賞賛
返信