Hi folks,
I'm using NXP QWKS - SCMIMX6DQ board while it is running on VxWorks 7,and I just want to run the OpenGL ES2 gear demo on VxWorks 7,but when I include the GPU drivers components,specially when I include the Freescale Vivante GPU kernel driver initialization (default),the VxWorks 7 will stop responding,the shell cannot input anything,when I objdump the Image ,find the PC pointer is stop at taskDelay function,so I guess where it is exist a endless loop,but I cannot determine where the mistake is,I use imx6q-sabresd.dts.
Hello Qiang Wu,
VxWorks is not supported on the i.MX BSP so I would recommend contacting Wind River for help with VxWorks.
I hope someone on the community may be able to help though.
Regards,