Hi,
Iam trying to add the QT5 for GUI development work.
I tried below
and I am getting error as below
also tried as per the reference manual
and compiled yocto using below command
fsl-image-qt5-validation-imx
and got the error as below
How can we resolve this issue
Regards
Santhosh
what backend do you build? x11 or wayland? try to use wayland to build qt5
Hi Joan,
I got this error when i compiled for QT5
Below is the packages added in local.conf
DISTRO_FEATURES_append = " x11 "
CORE_IMAGE_EXTRA_INSTALL += "opencv opencv-samples libopencv-core libopencv-imgproc"
CORE_IMAGE_EXTRA_INSTALL += "libopencv-core-dev libopencv-highgui-dev libopencv-imgproc-dev libopencv-objdetect-dev libopencv-ml-dev "
IMAGE_INSTALL_append = " gtk+ gtk+3 "
EXTRA_IMAGE_FEATURES += " libgtk2.0-dev pkg-config "
Hi Santhosh Kumar,
As mentioned in i.MX Yocto project user guide Rev. L4.14.98-2.0.0_ga, Frame buffer and X11 graphics are not supported in i.MX 8.
Regards,
Karan Gajjar
Joan,
I have used x11 to build
Regards
Santhosh