QSB not working with U-boot instructions. -blog archive

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QSB not working with U-boot instructions. -blog archive

629 次查看
captmark
Contributor I

If  follow the instructions from Quick Start Guide for i.MX54 QSB. It appears  that maybe the sync freq is not working. There is a column about 1/5 of the lcd width that has the lcd screen layered in it. I did test the lcd when I first received the kit and the lcd work fine out of the box. I am running same sd card that came with kit. Only change has been toset bootregs to setup lcd.

 

Any ideas.

 

Mar

标记 (1)
0 项奖励
回复
1 回复

581 次查看
VladanJovanovic
NXP Employee
NXP Employee

Can you share full output of the boot process (u-boot and Linux kernel)? Also kernel command line you're using? Also what display are you using?

 

Kernel parameters change sometimes between two BSP releases, so make sure you're using correct parameters for your setup.

0 项奖励
回复