QSB compatibility with large touch screens

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSB compatibility with large touch screens

2,452 Views
ChenYosfe
Contributor I

Hi,

 

I would like to use LCD touch screen larger then the 4.3'' MCIMX28LCD screen, and I wonder if there is such touch screen available that can be connected to the QSB as is (to the same socket as the MCIMX28LCD), without any hardware modification to the board. 

 

Thanks,

Chen

Labels (1)
0 Kudos
22 Replies

186 Views
ChenYosfe
Contributor I

Hi,

 

Thanks for the prompt response.

Is there a driver available for this touch screen as part of the Linux BSP ?

 

On another note - do you know if the QSB supports analog video input (for iPod out mode for example) ?

 

Thanks again,

Chen

0 Kudos

186 Views
SrikanthKotagir
Contributor I

Hi,

 

  The MCIMX-LVDS1 is a 10.1" Capacitive touch screen that can be used with the imx53QSB LVDS port.

0 Kudos