Hi,
I would like to use LCD touch screen larger then the 4.3'' MCIMX28LCD screen, and I wonder if there is such touch screen available that can be connected to the QSB as is (to the same socket as the MCIMX28LCD), without any hardware modification to the board.
Thanks,
Chen
Hi,
Thanks for the prompt response.
Is there a driver available for this touch screen as part of the Linux BSP ?
On another note - do you know if the QSB supports analog video input (for iPod out mode for example) ?
Thanks again,
Chen
Hi,
The MCIMX-LVDS1 is a 10.1" Capacitive touch screen that can be used with the imx53QSB LVDS port.