QSB HW reset button

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QSB HW reset button

1,947 次查看
AnthonyTong
Contributor I

I already own a QSB with Dialog DA9053 PMIC and today I received my new QSB with MC34708 PMIC. I found that I couldn't reset the board by pressing the reset button on the board. Did anyone have this issue before and what is the solution? Did I miss a patch to u-boot or kernel so the reset signal doesn't route to the chip correctly?

标签 (1)
0 项奖励
回复
4 回复数

1,665 次查看
MiroslavIMX53QS
Contributor I

I have a same problem with my QSB, and this is not deterministic behavior, sometimes it just works with one click, but the other times I have to hold a button longer.

0 项奖励
回复

1,665 次查看
AnthonyTong
Contributor I

I've just found out I need to hold a button for about 10 sec to reset. Thank you for your replies.

0 项奖励
回复

1,665 次查看
TheAdmiral
NXP Employee
NXP Employee

The reset button should be working on the MX53 Quick Start board. Are you using the same boot code for both boards? You need to be using the START-R code that came with the new board. The two codes are not compatible.

0 项奖励
回复

1,665 次查看
MiroslavIMX53QS
Contributor I

Did you try to hold a button pressed for some time (5 - 10 sec)?

0 项奖励
回复