QCA937x driver support in 4.1.x or 4.0.x kernels from NXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QCA937x driver support in 4.1.x or 4.0.x kernels from NXP

427 Views
mihaitaivascu
Contributor III

Hello,

    Does NXP provide support for the qca937x wifi driver in their 4.1.x or 4.0.x kernels?

    I could not find it. If not which would be the closest kernel version for it?

Thanks,

      Mihaita

Labels (1)
0 Kudos
1 Reply

313 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mihaita

>    Does NXP provide support for the qca937x wifi driver in their 4.1.x or 4.0.x kernels?

supported wifi is described in Release Notes document available in linux doc packages on below link,

unfortunately qca937x is not supported according to documentation.

i.MX Software|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos