Hi,
Thanks for your attenion.
We use I.MX53 running WEC7. The registery storage is "Hive-based Registry" and the file system is "RAM and ROM file system".
There are some problems need your help. Any suggestion is welcome, thanks!
Can anybody give any suggestion?
[Q2] The driver's loading order is not as we have set--[i.MX53-WEC7 ]
We want the display driver to be loaded befor backlight, so we set the platform.reg as below:
..........
;------------------------------------------------------------------------------
; GWES Display Driver
;
#if ((defined BSP_DISPLAY_DVI_TFP410 && defined BSP_I2CBUS2) || defined BSP_DISPLAY_CHUNGHWA_CLAA070VC01 || defined BSP_DISPLAY_VGA || defined BSP_DISPLAY_LVDS || defined BSP_DISPLAY_TVE)
[HKEY_LOCAL_MACHINE\System\GDI\Drivers]
"Display"="ddraw_ipu.dll"
"Order"=dword:10 ; load order
[HKEY_LOCAL_MACHINE\Drivers\Display\DDIPU]
"Bpp"=dword:10 ; RGB565
"VideoBpp"=dword:20 ; RGB666 (32bpp internal)
"VideoMemSize"=dword:8000000 ; 128MB
; @CESYSGEN IF CE_MODULES_COMPOSITOR
; Compositor Registry Configuration:
;
; CompositorPlugin SZ Plugin module name.
; FramePeriodMs DWORD Expected period, in milliseconds, for each render frame.
; DefaultOpaqueBpp DWORD Default pixel depth used when allocating window surfaces.
;
[HKEY_LOCAL_MACHINE\System\Gwe\Compositor]
"FramePeriodMs"=dword:20
"DefaultOpaqueBpp"=dword:10 ; 32bpp
; @CESYSGEN ENDIF CE_MODULES_COMPOSITOR
[HKEY_LOCAL_MACHINE\Drivers\BuiltIn\VDI]
"Prefix"="VDI"
"Dll"="vdi.dll"
"Order"=dword:20
"Index"=dword:1
#endif
;------------------------------------------------------------------------------
;------------------------------------------------------------------------------
; Backlight Driver
;
[HKEY_LOCAL_MACHINE\Drivers\BuiltIn\Backlight]
"Dll" = "backLight.Dll"
"Prefix" = "BKL"
"Flags"=dword:8 ;DEVFLAGS_NAKEDENTRIES
"Index" = dword:1
"Order" = dword:11 ; After display driver
"IClass" = multi_sz:"{F922DDE3-6A6D-4775-B23C-6842DB4BF094}",
"{0007AE3D-413C-4e7e-8786-E2A696E73A6E}"
;------------------------------------------------------------------------------
But when the system boot up, the driver's load order is not as we have set, why?
..........
PID:00400002 TID:01840006 +BSPBacklightInitialize
PID:00400002 TID:01840006 BKL::Backlight SPI Init.
PID:00400002 TID:01840006 -BSPBacklightInitialize
PID:00400002 TID:01840006 BKL::Sharememory Keypad
PID:00400002 TID:01840006 BKL::OK:CreateThread-g_hThreadKPBK
PID:00400002 TID:038D0002 ThreadProcKPBK ID = 0x38d0002
..........
PID:00400002 TID:01840006 GKP_Init:InterruptInitialize (dwSysIntr[i]-29,ISTEvent[i]-60817411) !
..........
PID:00400002 TID:01A40006 GKP::IOCTL_POWER_CAPABILITIES
PID:00400002 TID:01840006 ConfigOTGHost BoardId = 0x901
..........
PID:00400002 TID:03900002 BKL::Power state is = D0.
PID:00400002 TID:03900002 +BSPBacklightSetIntensity
PID:00400002 TID:03900002 BKL::Backlight to Level = +27
PID:00400002 TID:03900002 -BSPBacklightSetIntensity
PID:00400002 TID:04A6001E WARNING: possible performance issue: timeInit() not called, calling it in timeSetEvent()PID:00400002 TID:04A6001E BSPDisplayIOMUXSetup IOMUX setted.
PID:00400002 TID:04A6001E ===============DisplaySetMode===================.
PID:00400002 TID:04A6001E start initilization of LCD
PID:00400002 TID:04A6001E Initialize LD9042
PID:00400002 TID:04A6001E In CLAA.cpp set
..........