(Q2) Required queries about IMX6 ultra lite processor and its Errata. Need help for clarification

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

(Q2) Required queries about IMX6 ultra lite processor and its Errata. Need help for clarification

436 Views
ramesh6663
Contributor III

PMIC STBY_REQ Quires:
We used the PMIC 3001 (MC32PF3001A7EP) for our design. Since PMIC does not have PMIC_STBY_REQ dedicated pin. So, we have connected the Processor PMIC_STBY_REQ pin through MOSFET to make XTALI (T16) low.

Please see below snap shot from our schematic design.

Q3.png

1. Is this circuit really required only to make processor to be stand by mode?

2. How to make PMIC PF3001 in standby mode ? If there is any solution please provide us.

Thanks in advance

Thanks & Regards,

Rameshkumar

Labels (1)
0 Kudos
1 Reply

345 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ramesh

>1. Is this circuit really required only to make processor to be stand by mode?

No. It is optional circuit.

>2. How to make PMIC PF3001 in standby mode ? If there is any solution please provide us.Thanks in advance

Since there is no STANDBY pin in PMIC 3001, seems only way is to change voltages through I2C.
Please refer to below example:
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/drivers/regulator/pfuze100-regula...

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos