Putting TJA1043 to sleep after powerup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Putting TJA1043 to sleep after powerup

1,421 Views
balabalaji_kurr
Contributor I

Hi all,

We are using TJA1043 in our project, and facing an issue while sending the transceiver to sleep state.

 

After powerup, we are doing some diagnostics and based on the results, MCU is sent to sleep using SBC. So before calling SBC standby mode, all the CAN transceivers are sent to sleep mode.

 

I am following the sate machine defined in "AH1014 Application Hints - Standalone high speed CAN transceiver" document and also added below. I also read that in another post with the similar issue and in that it was mentioned to bring to transceiver to live state and then send the go to sleep command. I have done that and after sending the sleep command also polled for ERR and RXD pins. I always read "1", which is ok according the state machine.

 

I am not able find out what am I missing. Any hints would be appreciable.

pastedImage_1.png

Tags (1)
0 Kudos
Reply
1 Reply

1,352 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Balaji,

Please double check the following:

pastedImage_8.png

Go to Sleep mode.JPG

Fig. 4.JPG

pastedImage_7.png

Best regards,

Tomas

0 Kudos
Reply