Purpose of DQS dummy load on 8M Mini SOM reference design

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Purpose of DQS dummy load on 8M Mini SOM reference design

Jump to solution
2,439 Views
adevries
Contributor V

Hello,

On the reference design for the 8M Mini SOM, there is a capacitor connected to the NAND_DQS pin with the note "Dummy DQS for QSPI High Speed Timing" (see attached image). Can someone explain what the purpose of that capacitor is? How does it assist with QSPI High Speed Timing? Does the value of the capacitance matter?

I have a QSPI device that does not have a data strobe input, so can I just leave this pin unconnected? Or use it as a GPIO?

Thanks

Labels (1)
1 Solution
2,323 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  from Table 10-2 (External Signal List)  of i.MX 8M Mini  Reference Manual, Rev. 1, 03/2019:

Data Strobe signal Flash A (one of functions for this signal) :

• Loopback dummy read strobe:

FlexSPI controller provides internal dummy read strobe for flash read data. Higher read
frequency can be achieved by looping back  this dummy read strobe from pad. This pin
can be floated or put some cap loads on  board level to compensate DATA/SCLK pins load.

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
Reply
3 Replies
2,324 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  from Table 10-2 (External Signal List)  of i.MX 8M Mini  Reference Manual, Rev. 1, 03/2019:

Data Strobe signal Flash A (one of functions for this signal) :

• Loopback dummy read strobe:

FlexSPI controller provides internal dummy read strobe for flash read data. Higher read
frequency can be achieved by looping back  this dummy read strobe from pad. This pin
can be floated or put some cap loads on  board level to compensate DATA/SCLK pins load.

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos
Reply
2,323 Views
adevries
Contributor V

Hi Yuri,

Thanks for the info, that helps me understand the purpose of it. Do you know why an 18pF capacitor was chosen as the load? Does NXP provide any guidance on choosing the proper capacitor for that pin?

Thanks

0 Kudos
Reply
2,323 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I am afraid we do not have detailed recommendations regarding choosing the proper capacitor.

Regards,

Yuri.

0 Kudos
Reply