Pull Up resistor for SDIO interface on i.MX 6SoloX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Pull Up resistor for SDIO interface on i.MX 6SoloX

ソリューションへジャンプ
4,528件の閲覧回数
andy_kim
Contributor IV

Hello,

I've been checking i.MX 6SoloX Reference schematic and had a query about SDIO interface.

All of SDIO interface have pull up resistor only on SDx_DATA0 and SDx_CMD line.

I don't understand why pull up resistors applied only for two lines except the rest of SDx_DATA lines.

Shouldn't they all SDIO Data lines have pull up resistors?

 

Thanks,

Andy

0 件の賞賛
返信
1 解決策
4,492件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

You are welcome! Answering your question, the ones used in the design are the minimum required but it does not cause any harm implementing the other pull-ups. 

 

BR,

Ivan.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,513件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

At the booting process normally those pins are required to detect the change of the voltage (NVCC_SD4) switching from 1V8 to 3V1, so please keep them as they are in the design.

 

Hope it helps!

 

BR,

Ivan.

0 件の賞賛
返信
4,501件の閲覧回数
andy_kim
Contributor IV

Dear Ivan,

Thanks for your prompt reply.

Then, All of SD1 to SD4 port should be pull up for SDx_DATA0 and SDx_CMD to VCC_SD4? right?

 

Thanks,

Andy

0 件の賞賛
返信
4,493件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

You are welcome! Answering your question, the ones used in the design are the minimum required but it does not cause any harm implementing the other pull-ups. 

 

BR,

Ivan.

0 件の賞賛
返信
4,487件の閲覧回数
andy_kim
Contributor IV

Dear Ivan,

 

Thanks for your confirmation.

 

Andy

0 件の賞賛
返信